CONNECTIONS Blog

Revolutionizing Sprinkler Installation with InstaSeal® Technology

Written by Viking Group, Inc. | Jul 29, 2024, 6:19:30 PM

In an exciting development for the fire sprinkler industry, InstaSeal® technology is poised to transform the world of fire sprinkler installation. The InstaSeal family, which centers around a gasketed welded pipe outlet and the innovative "Torque-Assist" protective sprinkler cap, promises to streamline the installation process for sprinkler fitters across the industry.

The traditional fire sprinkler installation process has long been associated with the cumbersome use of wrenches, messy sealants and a time-consuming setup. However, with InstaSeal technology, all of that is about to change. This cutting-edge family is set to redefine the way fire sprinklers are installed and offers contractors a host of benefits that simplifies the installation process.

Game-Changing InstaSeal® Technology

The heart of InstaSeal technology lies in its gasketed welded pipe outlet and the "Torque-Assist" protective sprinkler cap. The InstaSeal gasket effectively seals the connection upon sprinkler installation, eliminating the need for additional sealants like PTFE tape or thread sealant, which are typically used in traditional installations. The "Torque-Assist" cap simplifies the process and allows for hand-tightening, removing the need for wrenches. 

 

Streamlined Workflows and Cost Savings

InstaSeal not only simplifies the installation process but also offers significant time and cost savings. With faster installations and reduced labor costs, contractors can work more efficiently and cost-effectively. InstaSeal is engineered for dependable, leak-free seals and is cULus Listed and FM Approved, meeting the highest standards of performance and dependability when used alongside Viking sprinklers.

Viking Sprinkler Compatibility

Select Viking sprinklers are compatible with the advanced InstaSeal® technology through the addition of new "Torque-Assist" caps. Make sure to look for the compatibility icon to ensure the correct sprinklers are being ordered for a job requiring InstaSeal technology.

Leading the way in Fire Sprinkler Installation

With innovative solutions like the gasketed welded outlet and "Torque-Assist" protective cap, InstaSeal is at the forefront of the industry, providing contractors with the tools they need to succeed.

For more information about the InstaSeal welded sprinkler fittings and Viking “Torque-Assist” cap, visit our website or contact your local Viking SupplyNet sales representative.

Check out this installation video to see just how easy it really is.

Availability

You can find InstaSeal technology at your local Viking SupplyNet fabrication and distribution center. Be sure to check with your local Viking SupplyNet representative. Customers should be sure to sign up for important updates related to InstaSeal to ensure they receive communications about availability in their region. Head to our landing page for more information!