Evolutionary shifts in regulations, particularly those aimed at the ongoing reduction of hydrofluorocarbons (HFCs) on a global scale, significantly impact the landscape of fire protection strategies. The decision to invest in a gas fire suppression system to safeguard high-value or irreplaceable assets should yield enduring benefits, rather than being deterred by the fluidity of environmental regulations. Prior to the availability of inert gas systems, clients often incurred substantial expenses associated with the removal or upgrading of systems to comply with evolving environmental standards or governmental mandates.
Through the utilization of Oxeo Extinguishing System's naturally occurring elements—argon or nitrogen—clients can adopt an inert gas suppression system in lieu of unsustainable synthetic alternatives. Given that inert gases are inherently present in the atmosphere, clients can be assured of the longevity and sustainability of this system, irrespective of regulatory changes or environmental legislation. Consequently, clients can confidently make an investment that aligns with a sustainable future.
Common Oxeo Applications
Oxeo Extinguishing System operates by reducing oxygen levels and cooling the affected area. In doing so, Oxeo disrupts two critical components of the "fire triangle," effectively thwarting the chemical reaction necessary for combustion, all while minimizing property damage. For a comprehensive understanding of the system's functionality, please refer to the animation below or on YouTube.com/vikingsprinkler, which provides a detailed illustration of its operation.
This system is cULus Listed and FM Approved to protect all of the traditional installations in various damage-sensitive applications such as data centers, art galleries, control rooms and more for Class A, B and C fires, following strict NFPA 2001 guidelines. Viking's Oxeo Extinguishing System can protect from fires in Class D environments as well, which involve combustible metals.
Want to learn more about Viking's Oxeo Extinguishing System?
Head to our website at vikinggroupinc.com, or check out all the resources here. If you want to quote your system, get a head start by utilizing vInert, Viking's premiere Oxeo calculating software, which allows users to design a complete Oxeo Extinguishing System and submit their bill of materials to their local Viking SupplyNet for ordering.